המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Why does frame size 6 ATV630 or ATV930 Process Drive not have mounting holes for a flange mount kit?
Issue:
Wondering why does frame size 6 ATV630 or ATV930 Process Drive not have mounting holes for a flange mount kit

Product Line:
ATV600 and ATV900 series drives.

Environment:
Frame size 6 drives without flange kit mounting holes.

Cause:
Re-design of drive.

Resolution:
When the ATV600 and 900 series drives were released, there were no flange kit available for frame size 6 drives, so the drive were not drilled and tapped to mount the kit.  The drives have been re-designed recently to have mounting holes pre-drilled and tapped to attach a flange mounting kit.  Currently, (June 2021) there is not factory flange kit available for frame size 6, but pre-drilled and tapped holes are included on the drive so that a custom made flange kit can be attached to the drive.  Currently there is no confirmed plans to produce a factory flange kit for this frame size drive but this may change in the future.