איך נוכל לעזור לך היום?

Is the VW3A3725 Bacnet option card compatible with the ATV900 Series Drives?

Issue:
VW3A3725 Bacnet option card compatibility with the ATV900 Series Drives

Product Line:
VW3A3725
ATV930, ATV950, ATV960, ATV980.

Environment:
ATV600 drives only

Cause:
Information unclear in current literature.

Resolution:
No, the VW3A3725 is not compatible with any ATV900 series. It is designed for the ATV600 family only.