איך נוכל לעזור לך היום?

What is the minimum firmware version of the ATV600 drive that is needed to use the VW3A3725 Bacnet card?

Issue:
What is the minimum firmware version of the ATV600 drive that is needed to use the VW3A3725 Bacnet card.

Product Line:
ATV600 series drives.

Environment:
All models, All serial numbers.

Cause:
Drive firmware must be of a certain level to properly operate the VW3A3725 Bacnet card.

Resolution:
A minimum firmware version of V1.8 on the ATV600 series drive is required in order to operate the VW3A3725 Bacnet MS/TP card.