המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is Easergy P3 Smartphone & tablet application and how can I install it?
Easergy P3 Smartphone & tablet application is a tool where you can with wireless communication using your smart phone or tablet connect and login to a Easergy P3 device which is connected to a wireless network. With the application you can monitor the device or do settings and control breaker.

Go to Google Play or Apple store and take search for “Easergy P3 SmartAPP” and choose install. After install you can find the icon in your applications folder and you can tap it to start the application. In order to get the login credentials, you need to first do the registration.