המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can you run a smaller test motor on a ATV630 and ATV930 drive?

Issue:
Running a smaller test motor on an ATV630 and ATV930 drive.

Product Line:
ATV630 and ATV930

Resolution:
You will need to set up the drive to run the smaller test motor.
Programming:
Main Menu
Complete settings:
Motor Parameters
Motor Control Type=  Set to V/F 5 Points

In Simply Start menu set up your motor amps and HP to size of the test motor.

Be aware that you can run a smaller motor as long as the motor parameters in the drive will adjust low enough for the motor's specs.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)