המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
ATV61 and ATV71 drives what are the ttHA high torque attained and ttLA low torque attained values in reference to torque?

Article available in these languages: Spanish

Issue:
ATV61 and ATV71 drives ttHA high torque attained and ttLA low torque attained values in reference to torque

Product Line:
Altivar ATV61 and ATV71 drives

Environment:
All

Cause:
Motor Torque in percent

Resolution:
The high torque attained and low torque attained are between -300 to +300 % of rated motor torque of the motor.   The default value is 100%.

[High tq. att.] (ttHA): Motor torque greater than high threshold [High torque thd.] (ttH)
v [Low tq. att.] (ttLA): Motor torque less than low threshold [Low torque thd.] (ttL)