המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
In SoMove why is "Compare Configurations" grayed out when working with an ATV630 or ATV930?
Issue:
So Move option "Compare Configurations" not working when using ATV630 or ATV930?

Product Line:
Altivar Process Drives

Environment:
SoMove software

Cause:
Unable to compare configurations of Process Drives

Resolution:
It's a known issue, comparing offline two .PSX files is not available for ATV6xx/9xx. This should be fixed in a future SoMove release.
You can make online 'Load from Device and Compare' only, to compare already opened project with the drive