המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Opening an '.sta' file for a CanOpen application returns the error 'The required application object reference...CanOpen_Option_Default ... signature is different'
Issue
Opening an '.sta' file for a CanOpen application returns the error 'The required application object reference...CanOpen_Option_Default ... SIGNATURE is different'

Product Line
Unity

Environment
Windows 10


Resolution
After importing the '.eds' file for a CanOpen deivce into the Hardware Catalog and opening an '.sta' file for a CanOpen application returns
the error 'The required application object reference <...CanOpen_Option_Default ...> signature is different'.

fargar



The following steps can be used to resolve the issue:.
  • Open the Hardware Catalog Manager
  • Delete the third party device.  This will delete '.eds' file from the catalog.
argra
agr
  • Build the Hardware Catalog
  • Open the '.sta' file.

Note: Opening of the '.sta' file by Unity Pro automatically updates the Hardware catalog including the equipment with the
correct signature.