המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can you program Jog Forward and Jog Reverse on the Altivar 630 and Altivar 930?
Issue:
Wants to program Jog Forward and Jog Reverse on the ATV630 and ATV930 drives.

Product Line:
Process Drive:
ATV600 series (ATV630, ATV650, ATV660, ATV680)
ATV900 series (ATV930, ATV950, ATV960, ATV980)

Environment:
All

Cause:
Application

Resolution:

The ATV600 series drives do not have a specific JOG function.  Consider using a preset speed if required.

For the ATV900 series, you will need to wire and program per listed parameters below:

Under Complete Settings :
1. In the Command and Reference Menu > Reverse Disable = NO
...By Default in 2 Wire Control DI1 is Run Forward
**(note: by default DI2 is your Reverse Input)

2. In the Generic Functions Menu > JOG > JOG=DI5, JGF=10hz

When you enable DI1 and DI5 the motor will run forward at 10hz, when you enable DI2 and DI5 with DI1 Low, the motor will run reverse at 10hz.  Always Stop by releasing DI1 or DI2 prior to switching directions.