המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Set up and program the ATV630 and ATV930 Process drive with Profinet using Telegram 1

Issue:
ATV630 and ATV930 set up and program for Profinet using Telegram 1
Programming and configuration Profinet using Telegram 1

Resolution:
See instructions below.
telegram 1
telegram 2

telegram 3

telegram 4

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

שניידר אלקטריק ישראל

קבצים מצורפים
ATV930 drive profinet FAQ example.pdf [153.73 KB]