המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
ATV61 in a E-FLEX, drive is running, but not the motor?

Issue:
E-FLEX ATV61 drive is in RUN status with output frequency and voltage, but the motor is not running.

Product Line:
ATV 61
E-Flex

Resolution:

If the E-Flex has the bypass feature, then there will be a TEST/NORMAL switch on the front.  It is possible that the drive may be in TEST mode which would mean that the output circuit to the motor is open.  The VFD Output phase loss feature is inactive, so the drive will be allowed to run.

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.