המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What terminal blocks can be used with a BMXDAI0805 I/O module?
BMXDAI0805 I/O module can be used with one of the following terminal blocks:

- BMXFTB2000 - Cage clamp
- BMXFTB2010 - Screw clamp
- BMXFTB2020 - Spring clamp

The terminal blocks will have to be ordered separatly, the BMXDAI0805 I/O module does not come with any terminal block.


If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-266-8705 – Option 1 or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)