המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What terminal blocks can be used with a BMXDAI0814 I/O module

BMXDAI0814 I/O module can be used with one of the following terminal blocks:

- BMXFTB2000 - Cage clamp
- BMXFTB2010 - Screw clamp
- BMXFTB2020 - Spring clamp

The terminal blocks will have to be ordered separately, the BMXDAI0814 I/O module does not come with any terminal block.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)