המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Which PME 2020 report templates are included with the base PME license by default and which ones require additional licensing?

Issue
What are the default report templates in PME 2020?

Product Line
Power Monitoring Expert 8.2 Standard Edition
Power Monitoring Expert 9.0
Power Monitoring Expert 2020

Environment
PME Web Application

Cause
To determine when a license is required to run a report

Resolution
1. The following are the default report groups that don't require a  license:
PME 8.2, PME 9.0 and PME 2020
- Energy Management
- General
- Power Quality
- Usage Trending

2. The availability of these report groups is subject to licensing:
PME 8.2
- Billing and Allocation
- Energy Analysis
- Equipment Performance
- Generator Performance
- Power Capacity
- Power Efficiency
- UPS Performance

PME 9.0
- Backup Power Management
- Billing and Allocation
- Billing and Allocation / IT Billing
- Breaker Performance
- Capacity Management
- Energy Analysis
- Energy Analysis / Energy Modeling
- Insulation Monitoring
- Power Quality Performance

PME 2020
- Backup Power
- Billing
- Breaker Performance
- Energy Analysis
- Insulation Monitoring
- IT Billing
- Power Capacity

Note: Contact a Schneider Electric representative for more information about acquiring a license.