המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the maximum number of characters supported by the PRINT_CHAR function in Unity Pro ?
Issue:
Maximum number of characters supported by the PRINT_CHAR function in Unity Pro/ EcoStruxure Control Expert


Product Line:
Unity Pro/ EcoStruxure Control Expert


Resolution:
The PRINT_CHAR function will support a character string of 1,024 bytes maximum.



If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)