המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How many Popups can be opened with Vijeo Designer V6.2?
Issue
What is the total amount of Popup screens that can be opened at one time in Vijeo Designer v6.2 Runtime?

Product Line
Vijeo Designer Runtime v6.2

Environment
Simulated or Physical Human Machine Interfaces (HMI)

Resolution
Up to 3 popup screens can be opened simultaneously with Vijeo Designer.
The keypad that appears when you touch a Numeric or String Display counts as one popup.

Requirement 1: The Popup Panel must be configured in a different windows.
In this example, Popup Panel 2 and 3 cannot be on the screen simultaneously because they are part of the "1: Window1" group.
However, since Panel 5 is in a separate window group "2: Window2", that means that:
a) Popup Panel 5 and Panel 2 can simultaneously be on the screen.
b) Popup Panel 5 and Panel 3 can simultaneously be on the screen.
Window Groups

Requirement 2: Persistent mode must be selected from the Property Inspector for all your Window Groups.
(Persistent Mode keeps the Popup displayed even if you change Base Panels on the HMI Runtime)
Property Inspector Persistent Mode for Window Groups

שניידר אלקטריק ישראל

קבצים מצורפים
VJD popups open.jpg [123.08 KB]