המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How do we determine the version of a VDZ file?

Issue:
Is there a way to know what version a Vijeo Designer VDZ file was last saved in?

Product Line:
Vijeo Designer (all versions)

Resolution:
In Vijeo Designer, when you import a VDZ file, you can determine the version it was last modified in by checking the Project's properties under the Vijeo-Manager. Ensure you click on the project tab in the Vijeo Manager first and then select the project you need to find the version for.

There will be two properties: Version created and version last modified.

Vijeo Manager

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)