המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How can you monitor the status of the digital inputs on the ATV630 and ATV930 Process drives?
Issue:
Monitoring the status of the digital inputs on the Process drives

Product Line:
ATV630 and ATV930

Environment:
All

Cause:
Wants to monitor the status of logic input DI11

Resolution:


Address 5202 will show the status of the logic inputs.   if you want to monitor DI11 its bit 11 of the 5202 address.

"IL1I
IL1R"     Bit 0:     Value of LI1.
Bit 1:     Value of LI2.
Bit 2:     Value of LI3.
Bit 3:     Value of LI4.

Bit 4:     Value of LI5
Bit 5:     Value of LI6
Bit 6:     Reserved (= 0).
Bit 7:     Reserved (= 0).

Bit 8:     Reserved (= 0).
Bit 9:     Reserved (= 0).
Bit 10:   Reserved (= 0).
*   Bit 11:         Value of LI11

Bit 12:   Value of LI12
Bit 13:   Value of LI13
Bit 14:   Value of LI14
Bit 15:   Value of LI15