המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
ATV630 - How do I display runtime in mins, not secs?
Issue:
How do I display runtime in mins, not secs? Can you change it only to mins or hours?

Product Line:
Altivar Machines, Altivar Process Drives

Environment:
All models and serial numbers

Cause:
Appears the drive automatically displays in secs, then mins and then hours. Appears it does not give you the option to change this.

Resolution:
The Altivar Process Drives automatically changes from seconds (until 59 sec), then to minutes (until 59 minutes), then hours. This cannot be presently changed at the present time, and there is not another solution or workaround.