המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the type of license available for Ecostruxure Secure Connect Adviser?
Types of License
The types of licenses available for purchase by customer are the following ones:

Secure Connect LinkManager
The Secure Connect LinkManager license allows a LinkManager User user to login to the remote GateManager via the web UI of the LinkManager Win OS software.

Secure Connect LinkManager Mobile
The Secure Connect LinkManager Mobile license allows a LinkManager Mobile user to login to the remote GateManager via the UI of a mobile app edited by Schneider Electric Inc.

Secure Connect SiteManager Basic, 2 Agents
The Secure Connect SiteManager Basic license allows a secure remote connection to the display unit and offers full control over the unit. A SiteManager agent is a set of parameters for define a type of connectivity (TCP/UDP ports, type of service, ...). With this license, up to 2 SiteManager agents can be defined for the display unit to which this license is attached.
An agent could be set up for each network interface if the display unit has multiple network interface.

Secure Connect SiteManager Extended, 5 Agents
The Secure Connect SiteManager Extended license provides a secure remote connection to the display unit and offers full control over the unit, and full control over any unit within a subnetwork of that unit. A SiteManager agent is a set of parameters for define a type of connectivity (TCP/UDP ports, type of service, subnetwork, ...). With this license, up to 5 SiteManager agents can be defined for the display unit to which this license is attached.
An agent could be set up for each network interface if the display unit has multiple network interface.

Secure Connect SiteManager Extended, 10 Agents
The Secure Connect SiteManager Extended license provides a secure remote connection to the display unit and offers full control over the unit, and full control over any unit within a subnetwork of that unit. A SiteManager agent is a set of parameters for define a type of connectivity (TCP/UDP ports, type of service, subnetwork, ...). With this license, up to 10 SiteManager agents can be defined for the display unit to which this license is attached.
An agent could be set up for each network interface if the display unit has multiple network interface.

Basic Remote Access
Basic remote access can be achieved thanks to either "Secure Connect SiteManager Basic" or "Secure Connect SiteManager Extended" license. A basic remote access is about secure remote connection to the display unit and full control over that connection to the unit (UDP/TCP ports, type of service, ...).

Bellow is an example of basic remote access.



Extended Remote Access
Extended remote access can be achieved thanks to "Secure Connect SiteManager Extended" license. An extended remote access is about secure remote connection to any subnetwork of the display unit and full control over these subnetwork connections of the unit (UDP/TCP ports, type of service, ...).

Bellow are examples of extended remote access.