המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Impossible to save the DTM catalog file is returned after attempting to update the catalog
Issue
Impossible to save the DTM catalog file is returned after attempting to update the catalog

Product Line
Unity

Environment
Windows 10


Resolution
The error message 'Impossible to save the DTM catalog gets returned after attempting to update the DTM catalog following the
installation of a third party (i.e., Endress and Hauser, Rosemont, etc.) DTM software.
yuuu



This issue will occur if there are too many DTM installed on the PC.
To resolve the issue:
  • Uninstall any DTM's that are not needed.
  • Run a registry cleaner.