איך נוכל לעזור לך היום?

What are the spacing requirements when mounting multiple ATV312 drives next to each other?

Issue:
What are the spacing requirements when mounting multiple ATV312 drives next to each other?

Product Line:
Altivar Machines, Altivar 312

Environment:
All models and serial number

Cause:
N/A

Resolution:
Please see the Mounting section on page 14 of the ATV312 Installation Manual (attached) for mounting requirements:


שניידר אלקטריק ישראל

קבצים מצורפים
ATV312_Installation_manual_EN_BBV46391_02.pdf [2.28 MB]
Mounting.png [63.83 KB]