איך נוכל לעזור לך היום?

How is the JOG function programmed on the ATV340 drive?

Issue:
How to program the ATV340 drive for JOG?

Product Line:
Altivar 340

Environment:
All

Cause:
N/A

Resolution:
From the main menu, select menus Complete settings -> Generic functions -> Jog.
Default settings as follows.
JOG    Jog assignment, set as appropriate
JGF    Jog frequency,    10 Hz.
JGT    Jog delay,    0.5 s.

See attached file.

שניידר אלקטריק ישראל

קבצים מצורפים
ATV340 JOG.pdf [135.48 KB]