המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can I play a live video in the new Magelis HMIG5U2 HMI like the XBTGTxx40?
To substitute old XBTGTxx40 MultiMedia , we have done successful tests with Analog camera on Magelis HMIG5U2.

Using a Analog/ USB converter  from Imaging Source Company ( ref =DFG/USB2pro ) you can connect Analog Camera PAL/NTSC to Magelis GTU with Open box HMIG5U2 ;
This converter is distributed worldwide.
  • You  can re-use the VijeoDesigner XBTGTxx40 application and to convert it on HMIG5U2 Box with selection of the same display size than XBTGT !
  • You have same Video functions : Live Video Display , Record & Replay functions
  • You have also to install manually  on the HMIG5U2 the Windows drivers from imaging Source to control the converter.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

שניידר אלקטריק ישראל

קבצים מצורפים
USB_TO_COMPOSITE CONVERTER.jpg [7.34 KB]