המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to connect the CT leads for an EMB and EME series meter?

Issue
How to connect the CT leads for an EMB and EME series meter?

Production Line
Energy Meter Basic model (EMB)
Energy Meter Extended Range model (EME)

Environment
Current Transformers

Cause
Connecting the CT leads to the terminals

Resolution

Attach the CT leads to appropriately colored CT input terminals, see CT wiring connection below depending on the installation application (3-phase, 4-wire; 1-phase, 3-wire; 1-phase, 2-wire):

  • red lead to red terminal
  • black lead to black terminal
  • yellow lead to black terminal

diagram of leads

Polarity is indicated, with the minus (-) terminals connected to neutral within the meter, but polarity is insignificant to the operation of the meter. Since the meter automatically detects phase reversal, so it is not necessary to orientate a particular side of the CTs toward the load.

See Energy Meter Instruction Bulletin, FA212755, for detailed installation instructions.