המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to disable Field Bus Monitoring on an ATV320 drive [video]
Question:
How to disable Field Bus Monitoring on an ATV320 drive

Product String Reference:
  1. Top Level > Product Category > Industry > Industry Control & Drives > Variable Speed Drives > Altivar 320.
  2. Top Level > PR_Product_OPS_Structure > Variable Speed Drives and Soft Starters > Low Voltage AC Machines Drives > Altivar Machine ATV320

Objective:
The objective of this video is to provide guidance of how to disable field bus monitoring on an ATV320 drive.



Product Line:
IDSDS – Speed Drives Systems.

Environment:
N/A

Resolution:
  1. Go to the COnF [Configuration Menu] and select “FULL”
  2. Scroll to “FLt” and press enter
  3. Scroll to “CLL” [Communications Module Parameter]
  4. Select CLL again
  5. Find “NO” to disable field bus monitoring