המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can you run multiple motor wires in the same conduit from Altivar Process drives?

Article available in these languages: Spanish

Issue:
Contractor installed six ATV630 drives.  They used three conduit runs, putting two sets of motor cables into one conduit run.  They are asking if this installation is going to cause noise or other interference.

Product line:
Altivar Machines, Altivar Process Drives

Environment:
All

Cause:
Installation manuals do not address the separation of motor cables.

Resolution:
It is recommended to have separation of motor cables between separate drives and motors.  Running motor cables together could possibly generate leakages and/or noise from one cable set to another.