המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How can I change the Nodename when cloning the controller application with SoMachine V4.3 / EcoStruxure Machine Expert via SD Card?

Issue
How can I change the Nodename of a Modicon M2xx PLC when cloning the controller application with SoMachine V4.3 / EcoStruxure Machine Expert via SD Card?

Product Line
SoMachine, EcoStruxure Machine Expert,
Modicon M241, M251, M262

Environment
Phsical PLCs

Resolution
This can be done by adding the following line in the script.cmd file in the SD Card before inserting it into the destination Modicon M2xx PLC.
The file is under \sys\cmd\script.cmd

The line to be added is:

SetNodeName "MyPLCNodeName"


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

שניידר אלקטריק ישראל

קבצים מצורפים
scriptcmd.jpg [55.53 KB]
gateway_newnodename.jpg [118.67 KB]