המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Why I got the message "Email ID already exists" when I register in the builder of Ecostruxure Augmented Operator Advisor for the first time?
At the first registration in the builder of Ecostruxure Augmented Operator Advisor you can get the following message:

It is probably because this email is already used for another Schneider web application (example: Machine Advisor)
All Schneider web application use the same login / password
So, in order to connect to Ecostruxure Augmented Operator Advisor, reuse the login password already create before for another Schneider Web Application