המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Advanced One Line Application errors after upgrading from PSE 7.20 to PSE 8.2
Issue
After upgrading from PSE 7.20 to PSE 8.2, the AOL application will not animate correctly. When looking into the AdvOneLineStatusLog.txt file there are many errors similar to the following:
ERROR: WriteListHandleToPLS: Unable to Write Tag zOL\*

Product Line
PowerSCADA Expert 8.2

Environment
PowerSCADA Expert Runtime

Resolution
PSE 8.2's Advanced One Line code requires that all zol variables use the UINT type. Open the variables.dbf file and ensure that all zol variables are using the UINT type