המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What would cause the ATV630 or ATV930 Process drives to trip out on a CFA error?
Issue:
What is the CFA fault code on the ATV630 or ATV930 Process drives?

Product Line:
ATV630 or ATV930

Environment:
All

Cause:
The monitoring function has detected an error on the digital input assigned to [CabinetCircuit A Assign].
CFA is active when the detected error duration is longer than [CabinetCircuit A Delay] FdA.

Resolution:
The fault can only appear if a cabinet input has been configured as Cabinet Circuit A error.
The stop type when the fault appears is configurable.
The acquisition time of LI is 2ms.
Probable cause:
The monitoring function has detected an error on the digital input assigned to [CabinetCircuit A Assign].
CFA is active when the detected error duration is longer than [CabinetCircuit A Delay] FdA.
Remedies:
• Check the connected device (door switch, thermal switch,…) and its wiring.
• Check the parameters CFAA (high/low assignment of the cabinet IO)