המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What are the new features in SoMachine Basic V1.6 SP2?
  • Cyber security improvements:
  • Improve application password strategy (CVE-2018-7790, CVE-2018-7791, CVE-2018-7792)
  • Protect against some incorrect Modbus requests (CVE-2018-7789)
  • Firmware update tool helps ensure controller is not in RUN state before starting the update. If in RUN state, a confirmation is requested
  • When deleting a drive(s) from the IO scanner configuration, the software tests the application for consistency and proposes to remove the deleted drive(s) from the respective function blocks
  • User-Defined Function Blocks ( DFB )
  • Additional project templates:
  • xSample_DataLogging_FB.smbe
  • xSample_ModbusTcp_IOScanner.smbe
  • xSample_TeSysU_1adv123.smbe
  • xSample_User-Defined_FB.smbe
  • xSample_User-Defined_Function.smbe