איך נוכל לעזור לך היום?

What is the recommended SQL live database size limit in PME?

Product Line
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024

Resolution
The answer depends on the user; on how much data they want to keep and also knowing their server specifications.
They need to keep in mind how the database's growth will affect the performance of the system based on what they have in the field and on the server.

To help better determine this information, use the following documentation linked below:

Database growth calculations

Once the amount of live data has been decided, use the following articles to help with database archiving, trimming, and maintenance
How to trim the PME database
How to set up recurring trims on the PME databases

שניידר אלקטריק ישראל

קבצים מצורפים
PME 8.2 - User Guide.pdf [2.18 MB]
PME 8.2 Design Guide.pdf [5.81 MB]