המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What do I do when I see Error 1392 "When using logged variable values, assign the variable to a data logging group." in the Vijeo Designer Feedback Zone?

Issue

Error 1392 "When using logged variable values, assign the variable to a data logging group." appears when a Vijeo Designer HMI project is built.

Product Line

Vijeo Designer v4.5+

Environment

Windows 7, Windows 10

Cause

When Error 1392 "When using logged variable values, assign the variable to a data logging group." appears, it means that a Variable designated for logging that was mandatory is no longer assigned . In working with data logging, you must assign the variable to a data logging group, which contains a set of properties that specifies the data collection method and data storage details for a variable.

Resolution

Assign the variable to a data logging group using the Data Details tab in the Variable Properties dialog box or in the Variable node's Logging Group column.