איך נוכל לעזור לך היום?

is it possible to use CMDTOOL with Window 7 64bit?

No the "CMDTOOL" is a 32 bit software.
The single way to configure a STXIBY100 coupler in modes "CMD to IBY" or "Unity to IBY" is to keep a PLC with a legacy OS Win7 32 bit for instance.