המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Is there a polarity protection into the Magelis iPC HMIBM range?
Goals and Symptoms
Customer would like to know if there any polarity protection into the Magelis iPC HMIBM range as this information is not included in the User Manual.
The goal of this resolution is to provide the information regarding the polarity
Causes and Fixes
HMIBMP and HMIBMU are the same design.
They have been designed with internal polarity protection and over voltage(38V) circuits and under voltage(16V) circuits.