המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Why using EcoStruxure™ Machine SCADA Expert, the value of real variable is different between PLC and EcoStruxure™ Machine SCADA Expert?
Due to "Floating Point Error" sometime there is a difference between the variable's value of the PLC and EcoStruxure™ Machine SCADA Expert (VijeoXL) runtime with the variable type REAL
In the following picture, the value in the PLC is 46.3 but EcoStruxure™ Machine SCADA Expert read 46.29999923706
To avoid this issue, need to use the function "Format" in EcoStruxure™ Machine SCADA Expert