איך נוכל לעזור לך היום?

Error “Impossible to create a new DTM object” is displayed adding a Sepam40/60/80 DTM in Control Expert V14.0.

After installing the Generic Modbus DDXML DTM library SV 2.03 and updating the DTM Catalog we can see that Sepam40, Sepam60 and Sepam80 DTMs (SV 02.08) are present.
Problem is that with the Ecostruxure Control Expert V14.0 when one of these three references is added the error message “Impossible to create a new DTM object” is displayed.

This is a known issue and a specific Control Expert HF will be published soon, ControlExpert_V140_HF0507367R.

Note: Other Devices DTMs coming with this Generic Modbus DDXML DTM library SV 2.03 are not concerned by this FAQ.