המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Connexium DRS Predefined Switch configuration profile C16
Issue
Connexium DRS (Dual Ring Switch) configuration C16 is a new predefined configuration profile for Ethernet RIO, made available in January 2019.
Configuration Filename: C16_RIOMainRingTx_RIOSubRingFx_DIOCloudsTxV1.3.cfg

Although similar to the C3 DRS predefined configuration profile, the C16 configuration profile uses copper wire ports 5 & 6 for the main ring and fiber ports 1 & 2 for the sub-ring.  All other ports remain the same.

Example



Product Line
The C16 predefined profile is used with Connexium Extended Dual Ring switches:
TCSESM063F2CU1 ConneXium extended dual ring switch that has 2 ports that support multimode fiber.
TCSESM063F2CS1 ConneXium extended dual ring switch that has 2 ports that support singlemode fiber.


Resolution
Install configuration file: C16_RIOMainRingTx_RIOSubRingFx_DIOCloudsTxV1.3.cfg