איך נוכל לעזור לך היום?

Vijeo Designer Runtime Manager always launches with "Welcome to Vijeo Designer Trial Edition"

Issue: Vijeo Designer Runtime Manager always auto-starts and displays the dialog "Welcome to Vijeo Designer Trial Edition"

Product Line: Vijeo Designer Runtime for iPC/Generic PC

Resolution: This dialog will always appear (even if you have registered the software) when you are running under a user account (ie non-administrator). To stop this message from appearing, you will need to log out of the user account, login as an Administrator and press the "Start/Yes" button on the dialog box "Welcome to Vijeo Designer Trial Edition". This will set a registry key to stop the dialog box from appearing again. Once this is set, you can log back in as the user account. The application will start as expected.