המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Removing Control Expert and installing Unity Pro.
Remove Control Expert either through the Control Panel - Program and  Features or
Start - Programs - EcoStruxure Control Expert - Control Expert - Remove Control Expert and Run as Administrator.
Reboot the PC.

In addition, the following folders must be manually removed when replacing Control Expert with a Unity Pro Version

Once Control Expert is removed, delete the following:

- Windows 7 (32 bits):
- C:\Program Files\Common Files\Schneider Electric Shared\Tlb
- C:\Program Files\Common Files\Schneider Electric Shared\Common
- C:\Program Files\Common Files\Schneider Electric Shared\SRCSDK
- C:\Program Files\Common Files\Schneider Electric Shared\SSTA

- Windows 7 (64 bits):
- C:\Program Files (x86)\Common Files\Schneider Electric Shared\Tlb
- C:\Program Files (x86)\Common Files\Schneider Electric Shared\Common
- C:\Program Files (x86)\Common Files\Schneider Electric Shared\SRCSDK
- C:\Program Files (x86)\Common Files\Schneider Electric Shared\SSTA