המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Data Center Expert | API Information
Issue:
StruxureWare Data Center Expert Application Programming Interface (API) Information

Product Line:
StruxureWare Data Center Expert (DCE)

Environment:
DCE (all versions)

Resolution:

Data Center Expert version 8.1.0 introduced the public DCE REST API. Instructions and use are available locally at
https://<server_address>/isxg/rest

Data Center Expert versions 8.0 and prior can find instructions here:

https://dcimsupport.ecostruxureit.com/hc/en-us/articles/360039289673-Data-Center-Expert-Web-Services-API

Please note that support for the API is provided at the forum pages here:
https://community.se.com/

DCIM support can only verify the protocols work with the software, and are unable to assist with organization configuration strings/settings.  It is expected the end user understand the methodologies and nuances of the connection protocol within their network.  Schneider Electric can only provide information stating the protocol has been verified and tested using the API platform without issue.