המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the different between suffix N4 and S6 of the ATV320 drive?
Issue:
Suffix N4 and S6 of the ATV320 drive

Product Line:
Altivar ATV320

Environment:
All serial numbers

Cause:
Customer is looking for a replacement for ATV320U22S6, and wanted to know if he can use ATV320U22N4.

Resolution:
The ATV320U22S6 has 575V 3 phase input voltage, and the ATV320U22N4 has 460V 3 phase input voltage.  Customer needs to verify the correct 3 phase input voltage to order the correct part number for the ATV320, even though they are the same HP.