המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is an ASF fault on an ATV340 and how do I correct it?
Issue:
Customer is experiencing ASF [Angle error] on an ATV340 series drive.

Product line:
ATV340 series.

Environment:
Synchronous motor is being used.

Cause:
For synchronous motors, wrong setting of the speed loop when the reference goes through 0.

Resolution:
 Verify the speed loop parameters.
 Verify the motor phases and the maximum current allowed by the drive.

This detected error can be cleared manually with the [Fault Reset Assign] rSF parameter after the cause
has disappeared.