המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What can cause an EEFI [EEPROM Control] Fault on an ATV340 series drive?

Article available in these languages: Spanish

Issue:
Is there a way to resolve an  EEFI [EEPROM Control] fault on an ATV340 series drive?

Product Line:
Altivar Machines, Altivar 340

Environment:
All models and serial numbers

Cause:
An error of the internal memory of the control block has been detected.

Resolution:
  • Verify the environment (electromagnetic compatibility).
  • Switch off the product.  Wait for the display to go blank, then wait 15 more seconds, then switch on the product.
  • Return to factory settings (*Only recommended if you have a backup of the  program stored in SoMove or an HMI)
  • Contact your local Schneider Electric representative.