המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How do we close all Vijeo Designer popup panels without specifying which individual panel to close?
Issue:
Looking for a way to close popup panels without specifying which individual panel to close?

Product Line:
Vijeo Designer all versions

Resolution:
Unfortunately, it is not possible to close all popup panels with a single switch in Vijeo Designer, unless you are able to navigate to another panel and come back.