איך נוכל לעזור לך היום?

ION7550 Series, ION7650 Series End of Commercialization (Obsolescence)

Issue
ION 7x50 series Obsolescence (obsolete) End of Commercialization

Product Line
ION7550 Series
ION7650 Series


Cause
Partial withdrawal of ION7x50 series advanced power meters.

Environment
End of commercialization and recommended replacement.

Resolution
Please see attached Change Notice Information Announcement. It includes key dates and recommended replacements.

Notes from the offer manager:
With the recent introduction of ION9000 power meters, it is now time to begin the withdrawal of the ION7550 and ION7650 series meters from the market. End of commercialization will be September 1st, 2019. Some configurations will continue to be available after that date. Please see the attached CN Info sheet for additional details.
The last date to buy quantities of 30 or more meters is June 1, 2019. The references being withdrawn will still be serviced or repaired for a period of 5 years after the end of commercialization, until September 1st, 2024. Technical support will continue indefinitely, as well as continued support in power monitoring software.

This internal announcement will be followed by announcements to a broader internal audience via the North American Product News group on Yammer, and external announcement to distributors via Channel Guide.

שניידר אלקטריק ישראל

קבצים מצורפים
ION7650 and ION9000_Comparison.pdf [3.76 MB]
ION7x50 PWP - NSH180001CNInfo.pdf [432.55 KB]
ION7650 Obsolescence Letter.pdf [96.59 KB]