המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
I am using EcoStruxure Control Expert Version 14. I have return my single license to the Schneider License Server many times, now it doesn't work anymore.
Issue

User has bypassed the limit to transfer the license . User has single license which means One seat only which is registered with Schneider Electric.

Product

EcoStruxure Control Expert V14

Environment

Windows 10 64 Bit Operating System

Resolution

A single seat license which is registered with schneider electric using www.se.com/licensing link.
This license has a limit of 7 returns only. If the user reached the limits or still wants to rehost to a different machine / PC
In this case the user should contact Software Registration Center ( SRC ).
In any case user can always contact local Country CCC.