איך נוכל לעזור לך היום?

BMXDDM3202K pin out diagram detail

Issue

This document provides additional clarity regarding the BMXDDM3202K 40 pin wiring diagram found in the Modicon X80 Discrete Input/Output Modules User Manual.

Product Line

BMXDDM3202K - a 24 VDC discrete 16 input/16 output IO module.

Resolution

Details added to diagram:
1. Orientation of the 40 pin male connector
2. Identification of pin numbers on the connector
3. External power supply + and - pin connections
4. Pin out numbers of the IO points (shown in red)

img1