המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Does the M340 processor come with a SD card?

⚠ CAUTION ⚠

The information provided in this FAQ being considered as confidential content, as it can be exclusively used internally.

This flag has been added automatically when the article is published with internal visibility only.

Issue:
Does the SD card come with the M340 Processor.

Product line:
All M340 processors

Environment:
EcoStruxure Control Expert

Resolution:
Yes, the BMXRMS008MP card is supplied with each processor